PTN36043, Can I cross SS1, SS2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PTN36043, Can I cross SS1, SS2?

879件の閲覧回数
Jeong
Contributor I

I plan to connect all USB SS lines using two PTN36043.
I want to use TX1 and RT2/TX2 and RX1 as a pair because the artwork design is distorted. Is there a problem with the operation when it is connected like this?
TX1 RX2 - PTN36043 #1 -
TX2 RX1 - PTN36043 #2 -

0 件の賞賛
返信
1 返信

855件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Could you please give the connection diagram?

 

0 件の賞賛
返信