PT3816EVM DIP settings

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PT3816EVM DIP settings

1,196 次查看
gmuhafeez
Contributor I

Hi, 


We are using the PTN3816EVM and giving input of 5k 60Hz signal with 5 meter DP cable at the Host and 5 meter DP cable at the Monitor end. We see that Using EVM brd and 5 meter cables Display doesn't come up. But we used one Cablematters Redriver(https://www.amazon.in/Cable-Matters-DisplayPort-Amplifier-Resolution/dp/B07D949F59) Link above works with 5 meter at the input and 5 meter at the output works. So Is there any setting we need to change at the DIP ? Can you please help us with it ? 


Thanks, 
Muhafeez

0 项奖励
回复
2 回复数

1,186 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Suggest don't use the DP cable longer than 3meters.

 

0 项奖励
回复

1,180 次查看
gmuhafeez
Contributor I

Hi, 

Thanks for your response. 
Yes it comes up with the cable less than 3m. 
But My question is Does PT3816EVM doesn't support more than 3m ? 

Thanks, 
Muhafeez

0 项奖励
回复