Need MC56F84543 Vdd power on ramp up specification/Delta

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need MC56F84543 Vdd power on ramp up specification/Delta

ソリューションへジャンプ
1,759件の閲覧回数
LaMoris
NXP Employee
NXP Employee

Hello Richy,

 

Delta Shanghai report that MC56F84543 is latched up by a tiny ramp up voltage 0V~0.4V input to ADC pin when power on. This tiny voltage can be measured on Vdd, Reset as well, which means the system send power to Vdd later than other pins. Customer need our Vdd power on ramp up specification to modify their H/W circuit. Thanks for help.

 

Project is Baidu server power 2000W PFC, socket is MC56F84543VLH, GIBC is 1-1P4H1MP, LTR is $223.36K.

 

The signal description of waveform as below:

CH1(Yellow)GPIOA6(Pin10), used for test toggle signal. High steady means DSC does not work.

CH2(Green): Vdd.

CH3(Red): ResetB.

CH4(Blue):12V power source to Vdd 3.3V.

22648_22648.jpg84543 latched up.jpg


Best Regards,

Moris Hsu

MCU FAE


ラベル(1)
タグ(3)
0 件の賞賛
1 解決策
1,386件の閲覧回数
richy_ye
NXP Employee
NXP Employee

Hi Moris, the VDD power ramp up is between 1 ms to 100 ms.

元の投稿で解決策を見る

0 件の賞賛
1 返信
1,387件の閲覧回数
richy_ye
NXP Employee
NXP Employee

Hi Moris, the VDD power ramp up is between 1 ms to 100 ms.

0 件の賞賛