NXP has RTOS for DSC series(mc56f83xxx or mc56f84xxx)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP has RTOS for DSC series(mc56f83xxx or mc56f84xxx)?

Jump to solution
1,101 Views
Lurkersoo
Contributor III

NXP has any RTOS example for DSC series(mc56f83xxx or mc56f84xxx)? 

thanks!

0 Kudos
Reply
1 Solution
1,078 Views
Lorenzo_Mch_IT
Contributor IV

Hello Lurkersoo,

AFAIK there are no RTOSes for DSC from NXP, on the other hand there is a port for FreeRTOS for TWR-56F8400 based on the same 56800EX core used in mc56f83xxx and  mc56f84xxx DSCs.

Check the following links ...

1) post on FreeRTOS forum with attached source code:


https://interactive.freertos.org/hc/en-us/community/posts/210026126-FreeRTOS-port-for-Freescale-DSC-...

2) More detailed explanation on how to use it and how to adapt it to other DSCs (or to newer FreeRTOS versions):

https://mcuoneclipse.com/2013/11/16/freertos-for-the-freescale-dsc-56f8400-core/

According to replies in the second link, it has also been successfully ported to 56F84789.

Lorenzo Micheletto

 

View solution in original post

0 Kudos
Reply
1 Reply
1,079 Views
Lorenzo_Mch_IT
Contributor IV

Hello Lurkersoo,

AFAIK there are no RTOSes for DSC from NXP, on the other hand there is a port for FreeRTOS for TWR-56F8400 based on the same 56800EX core used in mc56f83xxx and  mc56f84xxx DSCs.

Check the following links ...

1) post on FreeRTOS forum with attached source code:


https://interactive.freertos.org/hc/en-us/community/posts/210026126-FreeRTOS-port-for-Freescale-DSC-...

2) More detailed explanation on how to use it and how to adapt it to other DSCs (or to newer FreeRTOS versions):

https://mcuoneclipse.com/2013/11/16/freertos-for-the-freescale-dsc-56f8400-core/

According to replies in the second link, it has also been successfully ported to 56F84789.

Lorenzo Micheletto

 

0 Kudos
Reply