MCUXpress config build MC5683763 hello world that has MC56F83789 CMD ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpress config build MC5683763 hello world that has MC56F83789 CMD ?

Jump to solution
1,844 Views
547351265
Contributor II

SDK name :  SDK_2.7.2_MC56F83763.zip (From MCUXpresso SDK Builder )

MCUXpress config build hello world project (new project) of MC56F83763 .

Questions:1. The hello world project has MC56F83778 CMD ?

1.png

2. Debug failed as the picture:

2.png

3. 

0 Kudos
1 Solution
1,819 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Zhang,

I have only FRDM-56F83000 EVK board, I have tested on the EVK board, no problem.

Regarding your issue, do you use MC56F83763 or MC56F83789? I am confused, I think it is the problem. If you use MC56F83763, you have to create a MC56F83763 project.

BR

XiangJun Rong

xiangjun_rong_0-1606470061331.png

 

 

 

View solution in original post

0 Kudos
6 Replies
1,496 Views
sutter_zhou
NXP Employee
NXP Employee

Hi, @547351265 , please go to www.nxp.com/dsc , navigate to 56F83xxx product page, expand "Enablement" , you'll see below words:

sutter_zhou_0-1615800134021.png

This is the correct way to create a new SDK based project for any 56F83xxx parts. 

 

0 Kudos
1,769 Views
rooter344
Contributor I

The principle is to launch Eclipse in 'headless mode' using the ... Batch file to build an Eclipse project from the command line on Windows ... using CDT 9.4.3, using a project with two (Release/Debug) build configurations:.check here

0 Kudos
1,836 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Zhang,

It appears that I can not download the SDK package from the SDK builder link:

Can you post the SDK package so that I can have a test?

BTW, can you use the ***_SDM_LPM project and use OSJTAG port?

BR

XiangJun Rong

0 Kudos
1,827 Views
547351265
Contributor II

The private message has been sent to your hello world project .

It has no SDM_LPM, only LDM_LPM .

3.png

1.  MCUXpreeso SDK v2.7.2 from the picture 

2.png

2. build hello world by MCUXpresso Config Tools from the picture:

无标题.png

0 Kudos
1,820 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Zhang,

I have only FRDM-56F83000 EVK board, I have tested on the EVK board, no problem.

Regarding your issue, do you use MC56F83763 or MC56F83789? I am confused, I think it is the problem. If you use MC56F83763, you have to create a MC56F83763 project.

BR

XiangJun Rong

xiangjun_rong_0-1606470061331.png

 

 

 

0 Kudos
1,808 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

maybe you can use the MCUXpresso configure tools to clone a new project based on the SDK of MC56F83789, but I never have a test.

I attach the doc, pls refer to it.

If it can not solve the issue, I will report to SDK team

BR

XiangJun Rong

0 Kudos