SDK name : SDK_2.7.2_MC56F83763.zip (From MCUXpresso SDK Builder )
MCUXpress config build hello world project (new project) of MC56F83763 .
Questions:1. The hello world project has MC56F83778 CMD ?
2. Debug failed as the picture:
3.
Solved! Go to Solution.
Hi, Zhang,
I have only FRDM-56F83000 EVK board, I have tested on the EVK board, no problem.
Regarding your issue, do you use MC56F83763 or MC56F83789? I am confused, I think it is the problem. If you use MC56F83763, you have to create a MC56F83763 project.
BR
XiangJun Rong
Hi, @547351265 , please go to www.nxp.com/dsc , navigate to 56F83xxx product page, expand "Enablement" , you'll see below words:
This is the correct way to create a new SDK based project for any 56F83xxx parts.
The principle is to launch Eclipse in 'headless mode' using the ... Batch file to build an Eclipse project from the command line on Windows ... using CDT 9.4.3, using a project with two (Release/Debug) build configurations:.check here
Hi, Zhang,
It appears that I can not download the SDK package from the SDK builder link:
Can you post the SDK package so that I can have a test?
BTW, can you use the ***_SDM_LPM project and use OSJTAG port?
BR
XiangJun Rong
The private message has been sent to your hello world project .
It has no SDM_LPM, only LDM_LPM .
1. MCUXpreeso SDK v2.7.2 from the picture
2. build hello world by MCUXpresso Config Tools from the picture:
Hi, Zhang,
I have only FRDM-56F83000 EVK board, I have tested on the EVK board, no problem.
Regarding your issue, do you use MC56F83763 or MC56F83789? I am confused, I think it is the problem. If you use MC56F83763, you have to create a MC56F83763 project.
BR
XiangJun Rong