MC9S12XEP100MAL & S912XEP100W1MAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12XEP100MAL & S912XEP100W1MAL

Jump to solution
1,034 Views
glennarguil
Contributor I
Hi Sir / Madam Need your help regarding part no. MC9S12XEP100MAL & part no.S912XEP100W1MAL are both same function, & how to determine the clock frequency. Hoping for positive response. Thanks Glenn
0 Kudos
1 Solution
1,022 Views
StanoA
NXP TechSupport
NXP TechSupport

Hello Glennarguil,

The MC... mark means the MCU is mask independent for the specified type (S12XEP100).

The S...W1... mark means exact mask defined by W1 (mask set & revision).

The detail information about marking is in Reference Manual on: 

https://www.nxp.com/docs/en/data-sheet/MC9S12XEP100RMV1.pdf - Ordering information.

The clock frequency can be determined from RM / Chapter 11 also. It is valid for both mentioned marked devices.

If you need more help, you are welcome.

Best Regards,

Stano.

 

View solution in original post

0 Kudos
2 Replies
1,023 Views
StanoA
NXP TechSupport
NXP TechSupport

Hello Glennarguil,

The MC... mark means the MCU is mask independent for the specified type (S12XEP100).

The S...W1... mark means exact mask defined by W1 (mask set & revision).

The detail information about marking is in Reference Manual on: 

https://www.nxp.com/docs/en/data-sheet/MC9S12XEP100RMV1.pdf - Ordering information.

The clock frequency can be determined from RM / Chapter 11 also. It is valid for both mentioned marked devices.

If you need more help, you are welcome.

Best Regards,

Stano.

 

0 Kudos
1,014 Views
glennarguil
Contributor I

Thanks Stano. for the help 

0 Kudos