MC56F84xxx of ADC processor expert setting question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC56F84xxx of ADC processor expert setting question

跳至解决方案
1,731 次查看
Kris_Ke
Contributor III

Hi  

The datasheet show the 12-bit ADC frequency is 20Mhz.

frequency.PNG

When I setting the processor expert of the ADC, it always show "Warning : A/D frequency is too fast" and "Warning : A/D frequency 1 is too fast"

adc.PNG

 

No matter how you change the frequency, this warning will not disappear.

Did I miss anything that I didn’t set?

 

 

Thanks,

Kris

标记 (1)
0 项奖励
回复
1 解答
1,722 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kris,

I have tested to try to input different value for the "Clock divisor select value" box, the "warning: A/D frequency is too fast" always appears, so I think it is a bug of the PE for MC56F84xxx for CodeWarrior for mcu ver11.x.

Pls do not care about it.

BR

XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,723 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kris,

I have tested to try to input different value for the "Clock divisor select value" box, the "warning: A/D frequency is too fast" always appears, so I think it is a bug of the PE for MC56F84xxx for CodeWarrior for mcu ver11.x.

Pls do not care about it.

BR

XiangJun Rong

0 项奖励
回复