MC56F8006 - Low Frequency PWM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC56F8006 - Low Frequency PWM

1,675 次查看
CarlosCba
Contributor II

Dear,

 

Is possible to achieve a 10Hz frequency in the PWM module?

If is it possible, which are the correct settings?

 

Thanks.

标签 (1)
0 项奖励
回复
1 回复

1,537 次查看
johnlwinters
NXP Employee
NXP Employee


The general answer is of course this can be done.  However, what is the clock frequency you are running the system at?

It can be set to a very low frequency to save power.

HOW to do this will depend on what else you are doing at the same time; the complete system view would help, or as much as you can share.

If you wish to keep such confidential, I suggest using the technical information center support available at www.freescale.com.