MC33790

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC33790

2,624 次查看
MNRH
Contributor I

Hi,

We are using the MC33790 for establishing an a DSI1.0 communication with a sensor module MC33793

As per the document we have provided the circuit with the VCC as 5V and Vsup as 24V while sending the data the Idle voltage is coming only up to 11.5V, not 24V can someone explain to me why the idle voltage is not reaching the expected 24V. 

Thanks 

Rakesh 

0 项奖励
回复
6 回复数

2,480 次查看
MNRH
Contributor I

RakeshHegden_0-1656486130090.png

 

0 项奖励
回复

2,540 次查看
MNRH
Contributor I

Hi,

It was an issue with the DSIxF and DSIxS pin status if it is 1,0 respectively this issue occurs if it is set to 1,1 the VIDLE goes to 24V.

No it's not working with the MC33793 even after fixing the V Idle voltage issue  

 

0 项奖励
回复

2,591 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Does it work well if Vsup down to 11.5V?

0 项奖励
回复

2,480 次查看
MNRH
Contributor I

No, It won't work 

0 项奖励
回复

2,475 次查看
guoweisun
NXP TechSupport
NXP TechSupport

So your company is Dorman Products, right?

0 项奖励
回复

2,513 次查看
guoweisun
NXP TechSupport
NXP TechSupport
Please show your schematic here!
0 项奖励
回复