Hello,
I'm working on a product based on DSC 56F84789, I need to have deeper information about it.
Documents DSP56800ERM.pdf (DSP56800E and DSP56800EX Core Reference Manual), MC56F847XXRM.pdf (MC56F847xx Reference Manual, Rev. 2, 3/2016 ) and MCU_DSC_Compiler.pdf (CodeWarrior Development Studio for Microcontrollers V11.x Digital Signal Controller Build Tools Reference Manual, Rev. 11.x, 10/2019) contain lots of useful information and the same applies to the related application notes, but there are things missing or not very clear here an there.
I was wondering if it is possible (for example, by signing an NDA) to have access to more details, or even better, to the source code of DSC assembler, linker and compiler to check what's actually going on with some code I'm working on.