LA9310 unable to connect to CWIDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LA9310 unable to connect to CWIDE

3,055 次查看
varun0106
Contributor I

I am working on LA9310RDB, when i try to connect VSPA using cwide, it throws following error

"CCSProtocolPlugin::Can't connect to CCS"

I have configured the IP of jtag.

I also saw a link on the internet for the same, "https://community.nxp.com/t5/CodeWarrior-Development-Tools/Can-t-connect-CCS/m-p/459955"

But I am not able to understand anything from this, as it is a 6 year old post and CCS window is not there in CWIDE now

 

0 项奖励
回复
4 回复数

2,993 次查看
varun0106
Contributor I

Hi XiangJun,

Thanks for the reply,

Where do i have to execute these commands, i cannot fine command line window in the cwide

varun0106_0-1647425300665.png

 

0 项奖励
回复

2,985 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

It appears that you can not open the ccs menu, this is the screenshot which tells you how to open the ccs menu. I use the CodeWarrior for DSP56800E tools, but the menu is the same.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1647483642267.png

 

0 项奖励
回复

2,974 次查看
varun0106
Contributor I

Hi Xiangjun,

I started the CCS server manually from the cwide setup folder, then i started executing the commands which you have mentioned earlier, i got error in the third command "ccs::config_chain {la9310 dap}",

the error states "can't read "::ccs::core(la9310)": no such element in array,", what does it mean?

varun0106_0-1647520819212.png

 

0 项奖励
回复

3,027 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Varun,

This is an update to your question/request:

 

go to the ccs command line window and run the following command before you run the debug in CW

 

 

As you can see below VSPA is not in the jtag chain by default.

Once you do the write_mem commands below the VSPA is added to the jtag chain.

 

Good luck

 

bin) 61 % delete all

(bin) 62 % config cc cwtap:fsl042a86

(bin) 63 % ccs::config_chain {la9310 dap}

(bin) 64 % display ccs::get_config_chain

Chain Position 0: LA9310

Chain Position 1: Cortex-M4

Chain Position 2: CoreSight CTI

Chain Position 3: CoreSight CTI

Chain Position 4: CoreSight CTI

Chain Position 5: DAP

(bin) 65 % ccs::write_mem 0 0x41e60104 4 0 0x01000000

(bin) 66 % ccs::write_mem 0 0x41e60114 4 0 0x01000000

(bin) 67 % display  ccs::read_mem 0 0x41e6000c 4 0 1

                   +0       +4       +8       +C

[0x41E6000C] 01000000

(bin) 68 %

(bin) 68 % ccs::config_chain {la9310 dap}

(bin) 69 % display ccs::get_config_chain

Chain Position 0: LA9310

Chain Position 1: Cortex-M4

Chain Position 2: CoreSight CTI

Chain Position 3: CoreSight CTI

Chain Position 4: CoreSight CTI

Chain Position 5: VSPA2 core

Chain Position 6: DAP

 

Best Regards,

XiangJun Rong

0 项奖励
回复