Is it possible for the HCS12 XGATE to read two parallel lines of data?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible for the HCS12 XGATE to read two parallel lines of data?

713件の閲覧回数
danbocko
Contributor I

I am using an ADC that has two Data Outputs (DO and D1). Ch0 - Ch3 are output on D0 and Ch4 - Ch7 are output on D1 The maximum DCLK would be 32.768 MHz and the maximum Output Data rate would be 64KHz. Is it possible that the XGATE could read the simultaneous data on D0 and D1? Each data stream is 128 bits deep (4 channels * 32 bits per channel) The image below is the output using DCLK of 2.048MHz. If this can be done with the XGATE, is there an AP Note or something to get started.

Thanks

Dan

DataOutput.jpg

ラベル(1)
0 件の賞賛
返信
0 返答(返信)