Freemaster supports the connection with 56F8037 through JTAG or SCI interface.
User can use either Classic CodeWarrior v8.3 or Eclipse CodeWarrior v10.6 to develop the application which supports Freemaster connection.
Processor Expert contains two beans for FreeMaster communication, one is PC_Master, the other is FreeMaster. For SCI connection, you can choose either of them. For JTAG connection (using parallel or USBTAP), you can only choose FreeMaster.
Best Regards
Fiona
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Freemaster supports the connection with 56F8037 through JTAG or SCI interface.
User can use either Classic CodeWarrior v8.3 or Eclipse CodeWarrior v10.6 to develop the application which supports Freemaster connection.
Processor Expert contains two beans for FreeMaster communication, one is PC_Master, the other is FreeMaster. For SCI connection, you can choose either of them. For JTAG connection (using parallel or USBTAP), you can only choose FreeMaster.
Best Regards
Fiona
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------