Instruction addressing with DSC MC5684763 processor. 

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Instruction addressing with DSC MC5684763 processor. 

916 次查看
dalelee
Contributor II

I want to be able to store 2 images into program flash. One image is active image stored in location X1 and the other is a  backup image stored at location X2. The bootloader would select check if the active image is valid with CRC checksum. If for some reason it got corrupted, it would execute the old image.

 

The question is, can i execute the same image at different section of flash. Is the jump to function and variable an offset address or static address? How would i achieve in getting the same image to run from 2 different section of program flash? Is there a compile option? I do notice the routines and variables are copied into flash.

标签 (1)
0 项奖励
回复
0 回复数