Has anyone had success with the WAIT command on DSC 56F8300 family?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has anyone had success with the WAIT command on DSC 56F8300 family?

1,148 Views
Gus
Contributor I

I am using 56F8365 and STOP mode works fine but WAIT does not work.  The WAIT instruction acts like a NOP.  Verified conditions discussed in errata for STOP/WAIT modes when debugging and verified that wait_disable not active.

Labels (1)
0 Kudos
Reply
1 Reply

966 Views
johnlwinters
NXP Employee
NXP Employee

DId you try using the WAIT mode outside of the debugger?  Running the program with nothing attached to JTAG?

0 Kudos
Reply