Hi,
my target is S32k311 and I'm using Q-100 eval board. recently I added some code to my project which caused a HARD FAULT trigger.
we're using P&E USB MULTILINK debugger with GDB Eclipse, ever since I added the code that caused a HARD_FAULT .the debugger does not connect and this is what I get in the console:
Initializing.
Target has been RESET and is active.
Starting reset script (C:\NXP\S32DS.3.5\eclipse\plugins\com.pemicro.debug.gdbjtag.pne.expansion_5.5.7.202304031909\win32\gdi\P&E\supportFiles_ARM\NXP\S32K3xx\S32K310.mac) ...
REM Enable clocks for selected cores in MC_ME module (the sequence below enables all clocks).
REM Initialize RAM and DMA:
REM Initialize DMA TCD:
REM Copy valid executable code to RAM for each core to be used.
REM Enable required cores in MC_ME:
Delaying for 20mS ...
Done.
Reset script (C:\NXP\S32DS.3.5\eclipse\plugins\com.pemicro.debug.gdbjtag.pne.expansion_5.5.7.202304031909\win32\gdi\P&E\supportFiles_ARM\NXP\S32K3xx\S32K310.mac) completed.
BusFault: An imprecise (asynchronous) data access error has occurred.
HardFault: A fault has been escalated to a hard fault.
I do get the same error message even when I remove the code which caused this in the first place.
recycling the power and USB connections has no effect.
I need your assistance.
Regards,
Koorosh Hajiani