FORMAT DESFIRE EV1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FORMAT DESFIRE EV1

1,877 次查看
leonov_d
Contributor I

Hello, i can't format my desfair ev1 card, after authentication in app 00 (root) i send format command and recive next answer: f2 01 after which I can not use the card. How right format the card? I trying send cmd.Format + MAC(4 byte) + CRC16, and recive error 0x7E. 

标签 (1)
标记 (1)
0 项奖励
3 回复数

1,137 次查看
BSchaffer
Contributor I

Hello All,

I have the identical problem.   

Cards are overseas sourced and using MF3ICD41 ( so they say, but as per NXPs Tag info app.  ).

A few also came from a source at Amazon.com.  Card are only good for CSN once this occurs. 

Any native card command results in PCB 0xF2 followed by RC 0x01   ( 0xF2 0x01 ) 

Cards operate mostly okay other than this, as long as you don't run 0xFC of course. 

btw: system is a TI micro driving a 663 frontend. 

--Barry 

0 项奖励

1,793 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Leonov,

Can you tell us the part number and the tools you are using?

BR

XiangJun Rong

0 项奖励

1,793 次查看
leonov_d
Contributor I

Hi

regarding part number i can't give answer...

Tools: cc1310, clrc633, code composer studio and card desfire ev1

Can this problem be due to the part number?

0 项奖励