DSC FLASH PROGRAMMER ERROR ON WINDOWS 10 OS.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DSC FLASH PROGRAMMER ERROR ON WINDOWS 10 OS.

1,684 次查看
ashoksingh
Contributor I

`

we are using 56800E software to program controller (MC56F8247) with windows 7 os now we upgrade our pc to windows 10.now we are using freescale dsc flasher to program controller but we have facing error.    (ERROR 1:The Address 0x000080 is out of range given the space memory space parameters.)

0 项奖励
回复
1 回复

1,485 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ashok,

Pls refer to the memory map for MC56F82xx,  the P memory ranges from 0x0000 to 0x7FFF, the 0x8010 is outof P flash range. Pls check your  link file, which define the memory space.

BR

Xiangjun Rong

pastedImage_1.png

0 项奖励
回复