Change PWM value of PTN3460I through Linux PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change PWM value of PTN3460I through Linux PC

ソリューションへジャンプ
4,022件の閲覧回数
tommys
Contributor III

Hello,

We would like to change the PWM value of PTN3460I from a Linux PC through Display Port. We expected the PTN3460I to be recognized by the PC as an I2C(I2C-over-AUX) device (slave address 0xC0) but could not find the slave address. Is it correct to access via AUX-CH(DPCD) instead of I2C? The EDID could be read at the slave address 0x50. Please tell us the correct access method.

Thank you for your cooperation.

Best regards,
tommys

タグ(1)
0 件の賞賛
返信
1 解決策
3,989件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Tommy,

PTN3460I default PWM setting is 12 bit, so that the DPCD register 0x722/0x723 working range is 0x000 – 0xFFF.

0x000 means PWM duty cycle = 100%, so PWM = 3.3V. And 0xFFF means PWM duty cycle  = 0%, so PWM = 0V.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,007件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tommy,

Yes, you will have to to access via AUX-CH (DPCD register) instead of I2C if you want to change the PWM value of PTN3460I from a Linux PC through DisplayPort.

You will need to change DPCD register 0X722 and 0x723 via DP AUX channel to modify display brightness according to eDP (Embedded DisplayPort) specification v1.3 in below figures.

Picture.png

Picture 1.png

 

Best regards,

Tomas

0 件の賞賛
返信
4,001件の閲覧回数
tommys
Contributor III

Hello Tomas,

Thank you for the reply.

In case of PTN3460I, what are the maximum and minimum values ​​of brightness? We think 0x1000 is 0% and 0x0000 is 100%. Is it correct?

Best regards,

Tommy

0 件の賞賛
返信
3,990件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Tommy,

PTN3460I default PWM setting is 12 bit, so that the DPCD register 0x722/0x723 working range is 0x000 – 0xFFF.

0x000 means PWM duty cycle = 100%, so PWM = 3.3V. And 0xFFF means PWM duty cycle  = 0%, so PWM = 0V.

Best regards,

Tomas

0 件の賞賛
返信
3,967件の閲覧回数
tommys
Contributor III

Hello Tomas,

Thank you for your reply. I understand.

Best regards,
Tommy

0 件の賞賛
返信