Can't download program to flash on MC56F8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't download program to flash on MC56F8

2,406 次查看
sm0khey
Contributor III

Hello guys!

I am using CodeWarrior with UTAP for flashing the MCU. The problem i encounter is the following:

sm0khey_1-1718620887209.png

 

sm0khey_0-1718620862351.png

Also when i use the software for flashing with UTAP, i get the error :

Performing PROGRAM operation on MC56F8257 through the UTAP . . .
HawkV2: Core not responding

Also i can connect to the MCU and use the old version of the software.
I saw that i might have locked the flash, but nothing has worked so far. Any idea how to fix this?
It happened to 2 MCU's so far

标记 (5)
0 项奖励
回复
5 回复数

2,316 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I do not know if the usbtap device is okay or not.

This is the usbtap for once.

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

 

You can also use multilink universal from third party:

www.pemicro.com

I suppose you use your own PCB board, is your PCB board okay?

BR

XiangJun Rong

2,314 次查看
sm0khey
Contributor III

Yes, my PCB board is ok, i've tried on 3 more boards and still says that you cannot connect to the core. I believe it's a problem with the USBTap, but i can't seem to fix it

0 项奖励
回复

2,302 次查看
sm0khey
Contributor III

Turns out the problem is not in my USBTap. I've tried to download another .elf to another DSC and it worked, but still cannot flash the first 3 DSC's. Any idea what might be the problem? The program i wanted to flash included commands to delete blocks of flash memory. Could i have locked the MCU? Also i can still control the digital inputs/outputs of the DSC controller that i can't download a new flash.

Also:

sm0khey_0-1719412105289.png


When i restart the DSC still won't connect

标记 (1)
0 项奖励
回复

2,388 次查看
sm0khey
Contributor III

up

0 项奖励
回复

2,339 次查看
sm0khey
Contributor III

up

0 项奖励
回复