About non-overlap time of TEA2016AAT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About non-overlap time of TEA2016AAT

Jump to solution
4,544 Views
YorkZHU
Contributor I

Hello, I notice that in Chapter 18, the minimum non-overlap time is 200ns, but after calculating the deadtime of LLC under 300kHz, the optimal deadtime is 73ns. In this case, I hope you will give a constructive help or advice, how could I optimize the parameter. Thanks! 

0 Kudos
Reply
1 Solution
4,491 Views
guoweisun
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
6 Replies
4,494 Views
guoweisun
NXP TechSupport
NXP TechSupport

it doesn't include 150ns.

0 Kudos
Reply
4,493 Views
YorkZHU
Contributor I

The deadtime I get from external pin is 50ns or 200ns? 

0 Kudos
Reply
4,492 Views
guoweisun
NXP TechSupport
NXP TechSupport

200ns.

0 Kudos
Reply
4,479 Views
YorkZHU
Contributor I

Fine. 

0 Kudos
Reply
4,509 Views
guoweisun
NXP TechSupport
NXP TechSupport

You should follow this parameter specification of this IC.

0 Kudos
Reply
4,506 Views
YorkZHU
Contributor I

If I need MOSFET working in the best frequency, I have to set the minimum non-overlap time parameter by using RDK01DB1561 development programming board? 

Besides, I need to know whether the minimum non-overlap time 200ns contains the fixed HB intern delay time 150ns. I mean 150+50ns. Or 50ns contains HB intern delay time. 

YorkZHU_0-1646623595145.png

 

0 Kudos
Reply