I used the MC33816 IDE build the code for MC33816, but however I changed the Vboost voltage, from 24V to 65V. The Vboost always up to almost 80V, then the chip be broken. The mean is I can't control it. Can you help me?
Thanks!
I also encountered the same problem, I can't control the Vboost๏ผso I had to use a voltage regulator to protect the MC33816 from damageใ
Does anyone know of a solution to this problem๏ผ
Yep! I resolved it
How did you solve it? (=^ ^=)
Other configurations is default, The MC33816 IDE version is 2.3.1.0
Which kind of board do you test on? EVB or your own design board?
my own design board, The schematic refers to the official demo. And I wanna know If I used the default configurations on MC33816 IDE, Can I direct to test the board?
Suggest you test in EVB firstly,even if the default setting the Vboost can't up to 80V because of the maximum value is about 72V.