About MC33816 Vboost

cancel
Showing results for 
Search instead for 
Did you mean: 

About MC33816 Vboost

444 Views
Contributor II

I used the MC33816 IDE build the code for MC33816, but however I changed the Vboost voltage, from 24V to 65V. The Vboost always up to almost 80V, then the chip be broken. The mean is I can't control it. Can you help me? 

Thanks!

Labels (1)
7 Replies

327 Views
Contributor I

I also encountered the same problem, I can't control the Vboost,so I had to use a voltage regulator to protect the MC33816 from damage。

Does anyone know of a solution to this problem?

0 Kudos

327 Views
Contributor II

Yep! I resolved it

327 Views
Contributor I

How did you solve it? (=^ ^=)

0 Kudos

327 Views
Contributor II

Other configurations is default, The MC33816 IDE version is 2.3.1.0

0 Kudos

327 Views
NXP TechSupport
NXP TechSupport

Which kind of board do you test on? EVB or your own design board?

0 Kudos

327 Views
Contributor II

my own design board, The schematic refers to the official demo.  And I wanna know If I used the default configurations on MC33816 IDE, Can I direct to test the board?

0 Kudos

327 Views
NXP TechSupport
NXP TechSupport

Suggest you test in EVB firstly,even if the default setting the Vboost can't up to 80V because of the maximum value is about 72V.

0 Kudos