ADC16 problem of MC56F84789

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC16 problem of MC56F84789

2,170 Views
jero17
Contributor I

1. GPIOA11/ANC19 is the only input pin of ADC16

2.Input trans-conduct Amp shares the same VDDA of the DSC, 3.3Vdc

3. conversion time 4uS, Sample time 20=long

4.Init code:

setReg32(ADC16_SC1A, 0x1FUL);
setReg32(ADC16_SC2, 0x44UL);
setReg32(ADC16_SC3, 0x0eUL);
setReg32(ADC16_CFG1, 0x5cUL);
setReg32(ADC16_CFG2, 0x04UL);

5. Synchronous Triggered, DMA read

 

Problem:

1.After 2-10 days normal running, ADC16 result becomes noisy and unpredictable. And some fixed value like 0x07f7 or 0x1ff7 may come out frequently.(input amp and signal source are checked OK)

2. Meanwhile, other analog parts of the DSC such as ADC12 and DAC12 or Comparators work well.

3. Till now, there are at least 5 DSCs suffered from the same problem one by one.

 

Help please!

Labels (1)
0 Kudos
Reply
4 Replies

1,780 Views
ruvimelaver
Contributor II

Hello ,

Please advise date code of the part .

Thanks

Ruvi

0 Kudos
Reply

1,780 Views
jero17
Contributor I

Hi,

I am looking forward to your suggestion.

Thanks

Wang Jun

1031915144.jpg

0 Kudos
Reply

1,780 Views
mohammad_kamil
NXP Employee
NXP Employee

DTE: 1435 indicates it  year 2014, 35th Week of manufacturing

0 Kudos
Reply

1,780 Views
jero17
Contributor I

the 6th, last friday

0 Kudos
Reply