56F8257 I2C slave timming restriction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

56F8257 I2C slave timming restriction

856件の閲覧回数
daweiyou
NXP Employee
NXP Employee

Hi:

I want to ask question for 56F8257 I2C working as slave,

1.from the DS, the I2C only support up to 100Kbit frequency, does it also available for I2C slave mode?

2.The Processor Experter  tool could set I2C peripherals faster than 100KHz, is it wrong?

I2Cx_FREQDIV  doesn't wrote any restriction for SCL frequency.

3.if i2c work under slave mode, if the master driver SCL frequency fast than 100K, could any abnormal signal be possible? please help check below snapshot for I2C wave working under 250KHz as slave.

8257.png

0 件の賞賛
返信
0 返答(返信)