Micron’s Memory Solutions for the New i.MX 8 Microprocessor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Micron’s Memory Solutions for the New i.MX 8 Microprocessor

Micron’s Memory Solutions for the New i.MX 8 Microprocessor

NXP’s latest and most powerful Microprocessor requires the latest and fastest memories to keep it running efficiently. During this session, we will discuss the new memories supported on the new i.MX 8 processor family. For DRAM, this will include DDR4 and Low Power DDR4. For non-volatile memory this will include Octal SPI NOR (XccelaTM Flash) which offers up to 400MB/s as well as the latest eMMC 5.X devices that also support high speeds. These devices are offered with Commercial, Industrial or Automotive temperature and quality ratings. I will include a section on packaging technologies that can provide designers with innovative ways to reduce size. These include Package on Package and Multi-Chip Packages. This session will provide designers with the tools necessary to create state-of-the-art i.MX 8 systems. Micron will be giving away 2-1/2” 120GB SSDs to the first 50 attendees of this session.

附件
无评分
版本历史
最后更新:
‎06-27-2017 07:09 AM
更新人: