what is the resistor value on the MCF52259's reset state

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what is the resistor value on the MCF52259's reset state

815 次查看
junhu
Contributor I

if MCF52259 enter a reset state, its datasheet said "All signals have a pull-up in GPIO mode". my question is: what the resistor value is?

标签 (1)
0 项奖励
回复
1 回复

716 次查看
TomE
Specialist II

> what the resistor value is?

That isn't in the Reference Manual. It is an electrical characteristic of the chip, so it is in the Data Sheet.


Specifically "Table 13. DC Electrical Specifications":

    Weak internal pull Up device current, tested at VIL Max.  -10 to -130 uA.

The "pullup" may not be a linear resistor, but may be a current source. Given the above currents, it is somewhere between 25k and 330k measured to ground.

Tom