what is the resistor value on the MCF52259's reset state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the resistor value on the MCF52259's reset state

811 Views
junhu
Contributor I

if MCF52259 enter a reset state, its datasheet said "All signals have a pull-up in GPIO mode". my question is: what the resistor value is?

Labels (1)
0 Kudos
Reply
1 Reply

712 Views
TomE
Specialist II

> what the resistor value is?

That isn't in the Reference Manual. It is an electrical characteristic of the chip, so it is in the Data Sheet.


Specifically "Table 13. DC Electrical Specifications":

    Weak internal pull Up device current, tested at VIL Max.  -10 to -130 uA.

The "pullup" may not be a linear resistor, but may be a current source. Given the above currents, it is somewhere between 25k and 330k measured to ground.

Tom