uClinux on MCF5329EVB --> Problems with dBug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uClinux on MCF5329EVB --> Problems with dBug

2,257 次查看
jesortsan
Contributor I
Hi,
 
I'm following the AN3408 due to build a sample CGI application for the uClinux-targeting MCF5329EVB.
 
I'm trying to download the kernel image built with LTIB to the target board.
When I was setting the target board with dBug, suddenly the dBug doesn't recognize the characters that I type. For example, instead of a blank space (space bar) it reads a '0'. And it happens with almost all the keyboard keys. I don't know what could be happen... Any idea? How can I solve it? Is there any way of restart the dBUG to its initial values?
 
Thanks
Best regards
Jesus
标签 (1)
0 项奖励
回复
2 回复数

892 次查看
matt_waddel
Contributor I
Hi Jesus,

I've never had the problem you described, but if you think dBUG has been corrupted
there are instructions for recovering included with the LTIB release. 

In the original iso in the <mount>/Help/hardware/CFFlasher/ directory are prebuilt
bootloaders and the software necessary to recover dBUG.  The README.txt has
instructions.  This will also reset all the dBUG "set" values.

Regards,
Matt

0 项奖励
回复

892 次查看
jesortsan
Contributor I

The problem was that the board that I have to convert USB to RS232 had cracked down and it didn't work. But thanks to you, now I have a newer dBug version on the board.

Best regards

Jesús

0 项奖励
回复