number of endpoints available as USB device/ coldfire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

number of endpoints available as USB device/ coldfire

Jump to solution
1,367 Views
oolongtea
Contributor I

Hi, I wonder if there's any limit of endpoint I can use for my usb device.(undecided coldfire product)

Can the same endpoint number be in and out?

 

thanks!

Labels (1)
0 Kudos
Reply
1 Solution
1,257 Views
TomE
Specialist II

A quick search through the parametrics and picking the first chip listed, the MCF51JM128, and reading the USB chapter:

16.1.3 USB-FS Features

• USB 1.1 and 2.0 compliant full-speed device controller

• 16-Bidirectional end points

• DMA or FIFO data stream interfaces

Searching Freescales web site for <"bidirectional end point" USB> gets 57 hits. You can download and read from that list.

Tom


View solution in original post

0 Kudos
Reply
2 Replies
1,258 Views
TomE
Specialist II

A quick search through the parametrics and picking the first chip listed, the MCF51JM128, and reading the USB chapter:

16.1.3 USB-FS Features

• USB 1.1 and 2.0 compliant full-speed device controller

• 16-Bidirectional end points

• DMA or FIFO data stream interfaces

Searching Freescales web site for <"bidirectional end point" USB> gets 57 hits. You can download and read from that list.

Tom


0 Kudos
Reply
1,257 Views
oolongtea
Contributor I

perfect.  Thanks Tom

0 Kudos
Reply