mcf52233以太网设置应该用codewarrior里的哪个组件?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mcf52233以太网设置应该用codewarrior里的哪个组件?

289 Views
18311460468
Contributor II

Ethernet__LDD这个组件不支持mcf52233,我现在在自己设置相关寄存器,怎样操作更简单一点?

Labels (1)
0 Kudos
1 Reply

215 Views
miduo
NXP Employee
NXP Employee

Hi,

For the ethernet TCP/IP communications, the customer will need to implement TCP IP stack. Interniche TCP IP stack was ported to MCF5223x and is provided by NXP for free.

There was Ethernet Seminar back in 2006 on MCF52235, and all the seminar documents&software is available to download from NXP web page:

http://www.nxp.com/files/abstract/overview/TSP9133_CF_DNLD_WP.htm?tid=tcev

I'd recommend to download Coldfire Ethernet Seminar Presentation.

Software for the lab is available here:

Firmware and Labs Directory Structure

The documentation for Interniche TCP IP stack API is in the archive file.

The API should allow the customer to write some simple connect and send type applications.

0 Kudos