issue with SPI to Ethernet bridge AN3906

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

issue with SPI to Ethernet bridge AN3906

941件の閲覧回数
chary
Contributor I

I just want to know what is the optimal SPI buffer size I should use in the AN3906(serial to Ethernet bridge) software.

I have interfaced MC9S12XDP512 to MCF51CN128 through SPI and both are configured to work at max frequency.

The coldfire controller MCF51CN128 is configured as SPI slave.

 

Regards,

CHary

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

772件の閲覧回数
yibbidy
Contributor V

That's a good question CHary, but unfortunately it's something you'll need to arrive at as it totally depends upon your application and data that you are transcieving.  If your application is very responsive to clearing out the buffer and your data is small then you'll get away with a small buffer, and of the course the converse is true.  The maximum data size of an IP Datagram is 1500 bytes.

Sounds like an interesting project BTW.

Shaun

0 件の賞賛
返信