float the phy pins on MCF5223x if unused?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

float the phy pins on MCF5223x if unused?

1,271件の閲覧回数
daverj
Contributor I

I have a board with several MCF52233 chips, only one of which will be using the ethernet port.

 

Should the PHY_RXN, RXP, TXN, and TXP pins be left floating on the ones where the ethernet is not used?  Or tied to ground? Or tied to VCC with resistors? Or.....?

ラベル(1)
0 件の賞賛
返信
1 返信

698件の閲覧回数
MrBean
Contributor I

I think placing 50 Ohm pullups to Vdd on all 4 of them is on the safe side.

 

0 件の賞賛
返信