Without Ethrnet cable, takes mor etime to boot MCF5223X demo baord

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Without Ethrnet cable, takes mor etime to boot MCF5223X demo baord

472 Views
TVNAIDU
Contributor III

I am using Nichelite stack with MCF3223X Demo board, if I have Ethernet connected to board, boots faster (4 Seconds), I have LCD display to GPIO, LCD comesup after 3 Seconds it boots.

If I don't have Ethernet to baord, takes 20 Seconds to boot, takes 2 Minuest for LCD to comeup, any idea why it takes longtime without Ethernet cable?.


Labels (1)
0 Kudos
2 Replies

312 Views
mjbcswitzerland
Specialist V

Hi

 

I expect that the software is waiting for the link-up from the Ethernet to start working normally. It may have a timeout after 20s waiting and then allows the rest to start. You will need to remove any dependencies on the Ethernet Link-up and the LCD (etc.) if you want it to start irrespectively of the Ethernet state.

 

Regards

 

Mark

0 Kudos

312 Views
TVNAIDU
Contributor III

Thanks Mark, I adjusted counts.

There are 3 while loops, each one is 5 Sec, also if no ethernet, DHCP client keep on trying for 20 secs.

0 Kudos