Who can do me a favour about MC68332!!please!!!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Who can do me a favour about MC68332!!please!!!!

1,842 Views
prison_break
Contributor I
When I read the system integration module reference manual and one sentence I can't understand. It is "The state of the clock mode (MODCLK) pin during reset determines which clock
source the MCU uses. When MODCLK is held high during reset, the clock signal is
generated from a reference frequency. When MODCLK is held low during reset, the
clock synthesizer is disabled, and an external system clock signal must be applied."
 
So my question is how do I make MODCLK high or low during reset, is that connect a resistor between VDD and MODCLK pin?
Labels (1)
0 Kudos
4 Replies

476 Views
Nouchi
Senior Contributor II
Hello,


You just have to pull up or pull down with a 10k resistor (might be enough). You just have to take care of what you want to do with PF0 (shared pin with MODCLK).


Emmanuel
0 Kudos

476 Views
prison_break
Contributor I
thnak you so much!BugMan!! I am a chinese student, and I am learning MC68332.
 
GOOD LUCK FOR YOU!!!
0 Kudos

476 Views
Nouchi
Senior Contributor II
Hello,

MC68332 is a little bit outdated. If you can, you'd rather learn MCF523x family, which is the ColdFire family replacement. It include a new eTPU unit with a lots improvements (TPU probably made the 68332 success).

Regards,
Emmanuel
0 Kudos

476 Views
prison_break
Contributor I
Hello
 
I have heard about the coldfire, i am a beginner and we do not have a emluator and others useful books, I only down some user's manual, so study MC68332 maybe easier than coldfire. For anther reason that is my tutor's idea.
 
think you again!!!
best wishes to you!!!
0 Kudos