What is the minimum driving strength (mA) for external driver to properly do reset configuration of the ColdFire/MCF54418CMJ250 (pins: BOOTMOD[1:0], FB_AD[7:0])? Thanks.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the minimum driving strength (mA) for external driver to properly do reset configuration of the ColdFire/MCF54418CMJ250 (pins: BOOTMOD[1:0], FB_AD[7:0])? Thanks.

900 Views
davidwong
Contributor I

What is the minimum driving strength (mA) for external driver to properly do reset configuration of the ColdFire/MCF54418CMJ250 (pins: BOOTMOD[1:0], FB_AD[7:0])? Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

776 Views
TomE
Specialist II

MCF54418 Data Sheet.

"Table 5. MCF5441x Signal information and muxing" shows BOOTMOD[1:0] and FB_AD[7:0] don't have pullups or pulldowns. FB_AD[15:8] do have Pulls on Reset though.

Section "Table 11. I/O electrical specifications" gives the "Input Leakage Current" for the pins.

If you look at the Reference Manuals, they usually say things like "The logic levels for reset configuration on FB_AD[7:0] must be actively driven when BOOTMOD equals 01". Then you check the Reference Designs and the Development Modules and find they often just use pullup or pulldown resistors on these pins. I've noted this here:

https://community.nxp.com/message/100980?commentID=100980#comment-100980

Tom

0 Kudos
Reply