Use Freescale codefire52233 chip, use of official Ethernet test source, the Ethernet module can send and receive data, but use of PE configuration of the module, still use the official source code, the program does not send and receive data, how to solve

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use Freescale codefire52233 chip, use of official Ethernet test source, the Ethernet module can send and receive data, but use of PE configuration of the module, still use the official source code, the program does not send and receive data, how to solve

1,157 Views
lichenhuili
Contributor I

捕获2.PNG

The following additional test source code。

Original Attachment has been moved to: 52233-EPHY_1.rar

0 Kudos
Reply
2 Replies

953 Views
fangli
NXP Employee
NXP Employee

Hi,

What the Ethernet test code you used? Does the MQX been included? And what the CW version you used for?

0 Kudos
Reply

953 Views
TomE
Specialist II

Write some code to dump/print all the Ethernet controller registers, or even better, every control register the chip has.


Run that when it is working on normal startup. Run it again when it is running under the debugger and not working.

Look for differences.

Tom

0 Kudos
Reply