TCP/IP stack for MCF5222x family

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TCP/IP stack for MCF5222x family

1,603 次查看
senthil
Contributor I
Hi all,

Is there any TCP/IP stack available for MCF5222x family ?
Can TCP/IP Lite stack by InterNiche be used for MCF5222x family also?
If so what is the memory size it occupies?

Looking for your answers.

lntsenthil
标签 (1)
0 项奖励
回复
1 回复

672 次查看
mjbcswitzerland
Specialist V
Hi lntsenthil

The MCF5222x has USB on-the-go but no Ethernet interface. Therefore it is not normally used together with a TCP/IP stack.

The MCF5223X family with integrated EMAC and EPHY allow single chip embedded IP applications.

Look at the uTasker operating system with integrated TCP/IP stack (www.uTasker.com) which is free (including support) for non-commercial use. There is a demo online at http://212.254.22.36 requiring about 50k code, 12k SRAM and 32K File system as reference.

Regards

Mark Butcher

www.mjbc.ch / www.uTasker.com
0 项奖励
回复