Shortage of GPIO with 5223X, any better chipset in CF family?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Shortage of GPIO with 5223X, any better chipset in CF family?

ソリューションへジャンプ
1,376件の閲覧回数
TVNAIDU
Contributor III
We are shortage of GPIO with 5223x, any better CF family chipset?, also lot of application code and web pages developed with M52233DEMo, looking for some compatable chipset with more GPIO (80 pin will be better). thanks.
ラベル(1)
0 件の賞賛
返信
1 解決策
715件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

If you don't need high speed GPIO it is quite easy to extend using QSPI and shift registers.

 

Also the M52259, with Mini-FlexBus allows additional high-speed memory mapped IO to be added (up to 80MHz).

 

Regards

 

Mark

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
716件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

If you don't need high speed GPIO it is quite easy to extend using QSPI and shift registers.

 

Also the M52259, with Mini-FlexBus allows additional high-speed memory mapped IO to be added (up to 80MHz).

 

Regards

 

Mark

 

0 件の賞賛
返信