Regarding the End of Line Expected errors for pragma definition in coldfire

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding the End of Line Expected errors for pragma definition in coldfire

3,071件の閲覧回数
preetuabraham
Contributor III

Hi,

  I want to relocate a function to a RAM location. I referred AN4329 and used the  Method 1 but I am getting compilation errors as end of line expected for all the three pragama statements. . I did try another method as defined below under Method 2, I am gettign errors for end of line expected along with illegal or unsupported attribute

Please suggest what is the best or any alternative to relocate a function to a RAM location

Method 1

/////defined in .c file

#pragma define_section mySectionInRAM “.myCodeInRAM” far_absolute RX
#pragma section mySectionInRAM begin

void function1(void);

void function1(void)

{

--

 

}

#pragma section mySectionInRAM end

 

Method 2

#pragma section RX “.myCodeInRAM” data_mode=far_abs
//#pragma section mySectionInRAM begin

__declspec(section ".myCodeInRAM") void function1(void);

__declspec(section ".myCodeInRAM") void function1(void)

{

}

 

Also my linker file where I created new section myCodeInRAM

 

#/*
# * File: flash.dld
# * Purpose: Linker file for M5475EVB and M5485EVB
# *
# * Notes: Creates a Flash bootable image
# */

 

KEEP_SECTION {.vectortable}


MEMORY
{
boot (RWX) : ORIGIN = 0x00000000 , LENGTH = 0x00200000
text (RWX) : ORIGIN = 0x02001000 , LENGTH = 0x02000000
vector_ram (RWX) : ORIGIN = 0x20000000, LENGTH = 0x00000400 /* Vector table */
data (RWX) : ORIGIN = AFTER(text), LENGTH = 0
myram (RWX) : ORIGIN = AFTER(data), LENGTH = 0
bss (RWX) : ORIGIN = AFTER(myram), LENGTH = 0
}

SECTIONS
{
# Heap and Stack sizes definition
___heap_size = 0x100;
___stack_size = 0x100;

.vector_ram : {} > vector_ram

___MBAR = 0x10000000;
__MBAR = ___MBAR ;

___SDRAM = 0x02000000 ;
___SDRAM_SIZE = (8 * 1024 * 1024);

# ___SDRAM_SIZE = (16 * 1024 * 1024);

___SYS_SRAM = ___MBAR + 0x00010000;
___SYS_SRAM_SIZE = (32 * 1024) ;

___MCDAPI_START = ___SYS_SRAM;
___MCDAPI_SIZE = (12 * 1024);

___CORE_SRAM0 = 0x20000000 ;
___CORE_SRAM0_SIZE = (4 * 1024) ;
__CORE_SRAM0 = ___CORE_SRAM0;

___CORE_SRAM1 = 0x20001000 ;
___CORE_SRAM1_SIZE = (4 * 1024) ;
__CORE_SRAM1 = ___CORE_SRAM1 ;
__CORE_SRAM1_SIZE = ___CORE_SRAM1_SIZE;

___CODE_FLASH = 0x00000000 ;
___CODE_FLASH_SIZE = (32 * 1024 * 1024);
___FLASH = ___CODE_FLASH ;

___BOOT_FLASH = 0x00000000 ;
___BOOT_FLASH_SIZE = (2 * 1024 * 1024);

# ___VECTOR_RAM = ___SDRAM;
___VECTOR_RAM = ADDR(.vector_ram);


# ___SP_AFTER_RESET = ___CORE_SRAM1 + ___CORE_SRAM1_SIZE - 4;

.boot :
{
. = ALIGN(0x4);
_BOOT_BEGIN = .;
_VECTOR_BEGIN = .;
vectors_s.obj(.text)
_VECTOR_END = .;
mcf548x_lo_s.obj(.text)
mcf5xxx_s.obj(.text)
sysinit_c.obj(.text)
. = ALIGN(0x4);
_BOOT_END = .;
} > boot

_VECTOR_SIZE = _VECTOR_END - _VECTOR_BEGIN;

.text : AT(0x00010000)
{
. = ALIGN(0x4);
_TEXT_BEGIN = . ;
#vectors_s.obj(.text)
*(.text)
*(.rodata)
. = ALIGN(0x4);
___DATA_ROM = . ;
_TEXT_END = . ;
} > text

_TEXT_PHYSICAL = 0x00010000;
_TEXT_VIRTUAL = _TEXT_BEGIN;
_TEXT_SIZE = _TEXT_END - _TEXT_BEGIN;

.data : AT(0x00010000 + SIZEOF(.text))
{
. = ALIGN(0x4);
___DATA_RAM = . ;
*(.data)
*(.sdata)
*(.relocate_code)
*(.relocate_const)
*(.relocate_data)
. = ALIGN(0x4);
___DATA_END = . ;
} > data

_DATA_PHYSICAL = 0x00010000 + SIZEOF(text);
_DATA_VIRTUAL = ___DATA_RAM;
_DATA_SIZE = ___DATA_END - ___DATA_RAM;


.my_ram : AT(0x00010000 + SIZEOF(.text) + SIZEOF(data))
{
. = ALIGN (0x4);
___myRAMStart = .;
*(.myCodeInRAM)
___myRAMEnd = .;
. = ALIGN (0x4);
} > myram

_myRAM_PHYSICAL = 0x00010000 + SIZEOF(text) + SIZEOF(data);
_myRAM_VIRTUAL = ___myRAMStart;
_myRAM_SIZE = ___myRAMEnd - ___myRAMStart;

.bss :
{
. = ALIGN(0x4);
___BSS_START = . ;
*(.sbss)
*(SCOMMON)
*(.bss)
*(COMMON)
. = ALIGN(0x4);
___BSS_END = . ;
} > bss


___HEAP_START = .;
___HEAP_END = ___HEAP_START + (512*1024);
___SP_END = ___HEAP_END;
___SP_INIT = ___SP_END + (4*1024);
__SP_INIT = ___SP_INIT;

}

 

0 件の賞賛
返信
4 返答(返信)

3,060件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please try to change the lcf file with memory size.

For example:

2020-12-03_22-11-14.jpg

 

Mike

0 件の賞賛
返信

3,053件の閲覧回数
preetuabraham
Contributor III

Hi,

   Please suggest on those lines. I wil try to change as per your suggestiosn not sure it will fix end of line unexpected compilation errors

0 件の賞賛
返信

3,055件の閲覧回数
preetuabraham
Contributor III

Hi Hui,

Thanks for the update but I am getting pragama complication errors as End of line expected using code warrior when using pragma statements to relocate as per the the document mentioned

 

0 件の賞賛
返信

3,026件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Could you please help to post the error info screen copy?

I will check if there with any suggestion within internal system.

best regards,

Mike

0 件の賞賛
返信