Power supply connections for MCF52223

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power supply connections for MCF52223

1,708 Views
Harjit
Contributor II

I would greatly appreciate if someone who has one of these chips up and running can confirm the following:

* VSSPLL, VSSA and GND are all connected together in a star fashion. I think that is what the EVB/DEMO board schematics are trying to indicate.

 

I notice that VDDA and VRH are connected together on the demo boards. Are you seeing noise or is the ADC pretty clean? Or are you filtering the power going into VRH?

 

Thanks,

Harjit

Labels (1)
0 Kudos
Reply
1 Reply

1,183 Views
Dave_at_Mot
Contributor III

Yes, you can tie all the grounds you mention together.  In general though, you don't want to do a star ground.  Star grounds work best when you have high currents and low frequencies.  Microprocessor systems don't fit this description.  You should be using a single full ground plane with all grounds routed as directly as possible to the plane. 

 

I have a MC52233 based design where I use the AtoD converter and I've tied VDDA and VRH directly to the 3.3V supply.  I do have a pretty clean 3.3V though as I'm using a linear regulator from 5.0V down to 3.3 to run the Coldfire.  I don't think there is a universal correct answer on the analog supply.  If you have lots of digital stuff on the 3.3V or you use a switching supply you may want to put a series ferrite bead and some bulk decoupling on these pins.  It also depends on what you do with the AtoD.  I'm monitoring some low frequency process stuff, so I do averaging in software to remove noise.   If you are converting wider band signals such as audio, you can't apply this approach and you need to be more careful here.

 

Hope that helps.

0 Kudos
Reply