Power consumption of MCF54416CMJ250

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power consumption of MCF54416CMJ250

1,980 Views
sreejithrnair
Contributor I

@nxp 

Hi,

Could you kindly provide total power consumption of 

MCF54416CMJ250

0 Kudos
Reply
3 Replies

1,930 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer chapter 2.3 of MCF5441x datasheet about MCF5441x product power consumption.
For the total power consumption based on used modules, customer could use that specification to calculate the power consumption data.
For example: 
In run mode with nominal 1.2V the core power consumption is:
P=V(I)= 1.2(V) * 0.127(A)=0.15W

Wish it helps.

Mike

1,925 Views
sreejithrnair
Contributor I

Thanks Hui.

 

0 Kudos
Reply

1,961 Views
TomE
Specialist II

That depends entirely on what you have it connected to, what modules inside it you're using, which power modes it is in for how long and how you've programmed it.

Have you read Section 2.3 (Power consumption specifications) in the Data Sheet?

Tom

 

0 Kudos
Reply