Parallell mode ADC in MCF52221 using Processor Expoerts ADC-bean.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Parallell mode ADC in MCF52221 using Processor Expoerts ADC-bean.

751 次查看
AnteOO
Contributor II

Hi guys!

 

You know if it is possible to use the ADC-bean to measure Once Parallell simultaneous on two channels, let's say channel 2 anc 5 (on separate S/H-circuits ), and during the program runs, I want to change which cannels, to for say 3 and 6. Is there a method, or an easy way to do this using Processor Expert ? I know it's possible if i didn't have to change which cannel is measured, but it's crucial that I may change it at an arbitary time.

 

Hope you have any ideas!

 

Thanks!

Andreas

标签 (1)
0 项奖励
2 回复数

339 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

unfortunately, the ADC bean does not support switching channels for simultaneous measurement, however, as it has been suggested in previous posts, you can switch by directly writing to ADC registers before each measurement. But please note that this is possible only if you have disabled individual channel accessing method like MeasureChan.

 

For example, to switch to channels 3 and 6:

 

void main(void)
{

....

  (void)AD1_Measure(TRUE);
 
  /* ADLST1: ??=0,SAMPLE3=0,??=0,SAMPLE2=0,??=0,SAMPLE1=0,??=0,SAMPLE0=3 */
  setReg16(ADLST1,0x03);               /* Set ADC channel list reg. */
  /* ADLST2: ??=0,SAMPLE7=0,??=0,SAMPLE6=0,??=0,SAMPLE5=0,??=0,SAMPLE4=6 */
  setReg16(ADLST2,0x06);               /* Set ADC channel list reg. */

  (void)AD1_Measure(TRUE);
.....

 

best regards
Petr Hradsky
Processor Expert Support Team

0 项奖励

339 次查看
AnteOO
Contributor II

Is it possible to just write a method that changes ADLST1 / ADLST2-registers to just put the channel you want in queue and then use the generated Start-method by the ADC-bean ? Or am I overlooking something?

0 项奖励