Hello,
I would like to use the MCF52252 for a new project. I need the ability to secure the flash memory, in order that it is not possible to read the flash (BDM access disable), and the only accepted function is a mass erase (via backdoor access or Ezport access). When i click on the "i" icon, in the "freescale buy" page, i see the following page (see attached picture). I am a bit confused with the mention "without security".
Can somebody tell me the meaning of "without security" ?
Does this means it is possible to secure the flash of only some MCF5225x devices (not all) ?
Regards.
解決済! 解決策の投稿を見る。
> It is still not clear for me.
The "with security" and "FLASH" parts of the description have ABSOLUTELY NOTHING to do with each other. The "Description" is a very short "chip feature list"
Part Number MCF52252CAF66
Description 100LQFP 256K FLASH WITHOUT SECURITY
Long Description: Package is 100LQFP. There's 256k of FLASH. This chip DOES NOT have the CAU "Security Module".
Part Number MCF52255CAF80
Description 100LQFP 512K FLASH WITH SECURITY
Long Description: Package is 100LQFP. There's 512k of FLASH. This chip DOES have the CAU "Security Module".
So it is "256k FLASH <COMMA OR FULL STOP> WITHOUT SECURITY" and not "256k (FLASH WITHOUT SECURITY)".
Tom
I can't get to that page from the screen snapshot you've provided, so I can't check my ideas.
I find it a very confusing summary line too.
The MCF5225x range consists of parts 2, 4, 5, 6, 8, 9. The different parts have different amounts of RAM, ROM and certain peripherals, specifically the Random Number Generator and Cryptographic units.
Could you please see if the pages for the "56" and "59" DON'T have "without security" and the others do? In that case "256k FLASH WITHOUT SECURITY" really means "variant with 256k of FLASH memory, but without the CAU security module".
Searching for "without security" in other Freescale documents shows up the following document for the MPC8536E:
http://www.freescale.com/files/32bit/doc/errata/MPC8536ECE.pdf
That document doesn't explain "without security", but the Data Sheet details that it means "with and without the Security Engine".
Tom
Thank you for your answer.
The link is: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF5225X&nodeId=018rH3YTLC00M95448&ta...
The attached picture "info" shows where i click to see the "details" page.
Here is the "flash security" detail for each device:
Part Number MCF52252AF80
Description 100LQFP 256K FLASH WITHOUT SECURITY
Part Number MCF52252CAF66
Description 100LQFP 256K FLASH WITHOUT SECURITY
Part Number MCF52254AF80
Description 100LQFP 512K FLASH WITHOUT SECURITY
Part Number MCF52254CAF66
Description 100LQFP 512K FLASH WITHOUT SECURITY
Part Number MCF52255CAF80
Description 100LQFP 512K FLASH WITH SECURITY
Part Number MCF52256AG80
Description KIRIN3 144LQ 256K FLASH WITHOUT SECURITY
Part Number MCF52256CAG66
Description KIRIN3 144LQ 256K FLASH WITHOUT SECURITY
Part Number MCF52256CVN66
Description 256K FLASH WITH SECURITY
Part Number MCF52258AG80
Description KIRIN3 144LQ 512K FLASH WITHOUT SECURITY
Part Number MCF52258CAG66
Description KIRIN3 144LQ 512K FLASH WITHOUT SECURITY
Part Number MCF52258CVN66
Description 512K FLASH WITHOUT SUCURITY
Part Number MCF52258VN80
Description 512K FLASH WITHOUT SECURITY
Part Number MCF52259CAG80
Description KIRIN3 144LQFP 512K FLASH WITH SECURITY
Part Number MCF52259CVN80
Description 512K FLASH WITH SECURITY
Part Number PCF52255CAF80
Description 512K FLASH WITH SECURITY
Part Number MCF52258CVN66J
Description 512K FLASH WITHOUT SUCURITY
Part Number MCF52258VN80J
Description 512K FLASH WITHOUT SECURITY
Part Number MCF52259CVN80J
Description 512K FLASH WITH SECURITY
It says: MCF52252, MCF52259 and one of the MCF52256 have "flash security" !
It is still not clear for me.
Can you please tell me your mind ?
Regards.
> It is still not clear for me.
The "with security" and "FLASH" parts of the description have ABSOLUTELY NOTHING to do with each other. The "Description" is a very short "chip feature list"
Part Number MCF52252CAF66
Description 100LQFP 256K FLASH WITHOUT SECURITY
Long Description: Package is 100LQFP. There's 256k of FLASH. This chip DOES NOT have the CAU "Security Module".
Part Number MCF52255CAF80
Description 100LQFP 512K FLASH WITH SECURITY
Long Description: Package is 100LQFP. There's 512k of FLASH. This chip DOES have the CAU "Security Module".
So it is "256k FLASH <COMMA OR FULL STOP> WITHOUT SECURITY" and not "256k (FLASH WITHOUT SECURITY)".
Tom
Thank you very much for your extended explaination.
It is now clear for me.
Regards.
Bob
FWIW:
Looking at the 52259 chip, which does have the CAU, "cryptographic acceleration unit", the description is "with security"
EDIT: I just saw the bottom of your last post, you already knew this.....