MCF54454 with branch cache hangs my flexbus?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF54454 with branch cache hangs my flexbus?

2,507 次查看
AndyDaytona
Contributor I

Hi,

I am having trouble with sporadic reads to unmapped flexbus memory causing

the processor to hang until the bus monitor kicks it going again.

 

The accesses seem to come from the branch cache, something like

 

move.l #1000,a2

...

lea sdram_label,a2

jsr (a2)

 

will still have caused a flexbus access at address 1000.

 

Turning the branch cache off comes with a 10% performance decrease which is no good.

 

I can extend an auto acknowledging chipselect to cover flexbus memory, what if a2 would point to

internal peripheral space?

 

Does anyone know if I am right about this? If so, can instruction prefetch disturb the internal peripherals?

 

 

best regards

 

Andy

标签 (1)
0 项奖励
回复
6 回复数

2,290 次查看
jkmahan
Contributor III

Does it still happen if you do a flush on the branch cache?

0 项奖励
回复

2,290 次查看
AndyDaytona
Contributor I

If I flush the branch cache in the kernel thread dispatcher, the problem seems to disappear (or happen so seldom

I cannot detect it, although I cannot detect it directly by stepping thru code, and I cannot get any bus error to detect this so I

cannot trace exactly what happens, it has taken almost two weeks to find this problem as I initially assumed that it was a code bug.)

 

from my disassembly I have this generated by gcc

 

loop:

jsr (a3)

jsr (a2)

addq.l #4,sp

bra loop

 

a3 points to the semaphore wait command

a2 points to something that executes every time I get a semaphore signal.

 

The pop is for the semaphore wait, but has been deferred.

When this code executes there seem to be a flexbus read at the address pointed to by a2 in another thread!

If I put just a trapf between the jsr instructions the problem goes away.

 

I have  a memory mapped external peripheral (a DSP) and if a2 for some reason would point to its memory,

it would be really bad. :smileysad:

 

 

0 项奖励
回复

2,290 次查看
jkmahan
Contributor III

Sounds similar to a problem I tracked down a couple of years ago when I worked for FSL doing the V4 Linux BSP.   

0 项奖励
回复

2,290 次查看
AndyDaytona
Contributor I

That sounds very interesting, did you manage to pinpoint how to avoid the problem?

 

I also noticed now that disabling the branch cache in cacr did not solve the problem.

 

I also managed to induce false reads to the ATA FIFO, hanging the DMA handler, using this

problem which proves that it is not isolated to the flexbus, I think.

 

This only leaves avoiding the instruction combinations creating this state altogether as an option.

0 项奖励
回复

2,290 次查看
jkmahan
Contributor III

The big issue was that I was changing the the MMU mappings and not flushing the branch cache at the same time I was flushing the other caches.  So there was stale data in the branch cache.

0 项奖励
回复

2,290 次查看
AndyDaytona
Contributor I

Ok, unfortunately, we do not use the MMU, so that shouldn't be it.

0 项奖励
回复