MCF5307 and 16bit flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5307 and 16bit flash

ソリューションへジャンプ
2,066件の閲覧回数
angelo_d
Senior Contributor I

Hello all,

 

i am booting colilo from a a 16 bit flash. Code is run correctly, but texts are printed out from the serial uncorrectly, due to the 16-bit word addressing mode:

 

Hello world is printed as HHeelloo  ..  

 

This becouse char* increment don't point to the next byte but to the same word.

 

Every help is really appreciated.

 

spectrum

ラベル(1)
0 件の賞賛
返信
1 解決策
1,365件の閲覧回数
angelo_d
Senior Contributor I

Hello all,

 

mm, i finally clarified the mistery: it is related to the flash 2Mx16 SST 29VF3201B i have chosed.

 

Unfortunately, even if the pinout is exactly as a correspondent size AMD x16 flash, i discovered that SST flash don't suport the x8 mode, or better, don't have the BYTE# signal on pin 47, but it is a NC.

 

I choosed SST for good pricing, and would avoid to replace it, so i am going to try to modify the colilo bootloader to copy rodata to rom.

Anyway this is just a beginner erro i guess :smileyhappy:

 

 

Hope this can help soem other,

 

greetings,

angelo

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,366件の閲覧回数
angelo_d
Senior Contributor I

Hello all,

 

mm, i finally clarified the mistery: it is related to the flash 2Mx16 SST 29VF3201B i have chosed.

 

Unfortunately, even if the pinout is exactly as a correspondent size AMD x16 flash, i discovered that SST flash don't suport the x8 mode, or better, don't have the BYTE# signal on pin 47, but it is a NC.

 

I choosed SST for good pricing, and would avoid to replace it, so i am going to try to modify the colilo bootloader to copy rodata to rom.

Anyway this is just a beginner erro i guess :smileyhappy:

 

 

Hope this can help soem other,

 

greetings,

angelo

0 件の賞賛
返信