I'm running the MCF52259 on my own board with a 48 MHz crystal. Npormally, I'm dividing down to 8 MHz, then multiplying up to 80 MHz. Here's the code I run out of reset:
MCF_CLOCK_CCHR = 0x05; // The PLL pre divider - 48MHz / 6 = 8MHz
MCF_CLOCK_SYNCR = MCF_CLOCK_SYNCR_MFD(3) | MCF_CLOCK_SYNCR_DISCLK | MCF_CLOCK_SYNCR_CLKSRC| MCF_CLOCK_SYNCR_PLLMODE | MCF_CLOCK_SYNCR_PLLEN ; //80 MHz clock
while (!(MCF_CLOCK_SYNSR & MCF_CLOCK_SYNSR_LOCK))
{
}
So far, so good. Now I'm trying to change the PLL setting once the processor is running (in order to reduce power con sumption). In order to do this, I change the CCHR pre-divider to 8 (7+1), MFD to 0 and RFD to 7, resulting in a system clock of: 6MHz / 32 = 187500 Hz. Replacing the previous startup code:
MCF_CLOCK_CCHR = 0x07; // The PLL pre divider - 48MHz / 8 = 6MHz
MCF_CLOCK_SYNCR = MCF_CLOCK_SYNCR_MFD(0) | MCF_CLOCK_SYNCR_RFD(7) | MCF_CLOCK_SYNCR_CLKSRC| MCF_CLOCK_SYNCR_PLLMODE | MCF_CLOCK_SYNCR_PLLEN; //6 MHz / 32 = 187.5 kHz clock
while (!(MCF_CLOCK_SYNSR & MCF_CLOCK_SYNSR_LOCK))
{
}
which appears to run just fine. I am able to use this system clock as input to the RTC with MCF_RTC_RTCGOCL = 0xB71B and this causes my little LED to blink happily at 1 Hz.
So now I try this same code while running at 80MHz. This time, there are no more happy blinky-LEDs. The power draw does go down, but this may be because the system clock is not functioning. If I set a debugger breakpoint at the while () loop, I get a trace/breakpoint exception. If I don't set a breakpoint, I get nada. I't not stuck in the while() loop; it;s not even getting to the loop. Just seems like the PLL fails to lock and the core stops executing instructions. after the write to MCF_CLOCK_SYNCR.
According to the Ref Manual, changes to RFD should not cause the PLL to lose lock, so I tried tried limiting the changes to RFD and leaving MFD alone, to no effect. I also tried disabling the PLL before making changes, but this did not do it either.
I might try making moire gradual changes to frequency, say one RFD or MFD value at a time, in the hopes that a gradual change will be easier to recover from. The documentation seems to indicate that when the PLL loses lock, it's just a matter of time before it will eventually regain lock.
Any ideas?
Thanks,
Yaniv
Solved! Go to Solution.
I did get it to work in the end by avoiding changes to CCHR. Changing MFD and RFD works just fine and the PLL regains lock. I was able to transition from 80MHz down to 250 kHz and back with no issues.
I did get it to work in the end by avoiding changes to CCHR. Changing MFD and RFD works just fine and the PLL regains lock. I was able to transition from 80MHz down to 250 kHz and back with no issues.
I would not be comfortable with adjusting PLL on-the-fly. When PLL is unstable, you can have out-of-spec (too short) pulses at CPU clock input. Such pulses can lock up the CPU.
You should switch to a different clock source, adjust the PLL, and switch back to PLL as clock source.