MCF52258 Not running without debugger attached

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCF52258 Not running without debugger attached

跳至解决方案
2,191 次查看
RxScram
Contributor I

Hi Everybody,

 

I've searched through the forums and found similar problems, but I didn't think any of the other problems were relevant.

 

My problem is this:  I have programmed the flash in my 52258, and if I run it with the BDM attached, it works fine.  However, if I try running it without the BDM, it does not run.  The interesting thing is that I do not do anything with the BDM... I just have it plugged in, without even having codewarrior running, and then I turn on the power and it runs fine.  If I turn off the power, unplug the BDM, and turn the power back on then nothing happens.

 

I think this could be a hardware design problem on my part, but I am not sure what it could be.  Any suggestions?  My BDM pinout is as suggested by the MCF52259RM document, and is basically identical to the eval board.  Since the BDM works great, I don't think that the error is in that portion.

 

Thank you.

标签 (1)
0 项奖励
回复
1 解答
1,292 次查看
scifi
Senior Contributor I

This problem should be easy to solve.

Assuming signals from the debugger are static, attach the debugger and write down the voltage levels it supplies to the MCU. Then detach it and do the same. You should now see what changed.

I have a MCF52259-based design running. No surprises, works like a charm.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,293 次查看
scifi
Senior Contributor I

This problem should be easy to solve.

Assuming signals from the debugger are static, attach the debugger and write down the voltage levels it supplies to the MCU. Then detach it and do the same. You should now see what changed.

I have a MCF52259-based design running. No surprises, works like a charm.

0 项奖励
回复
1,292 次查看
RxScram
Contributor I

Thanks, I should have done that on my own first.  I needed to add a pull-up on /bkpt, it was as simple as that.

0 项奖励
回复
1,292 次查看
trusc
Contributor II

I had the same problem on a board using the MCF52255. Problem solved after reading your posts.

 

Thanks - I'm pretty pleased about having found a solution to this problem! :smileyhappy:

0 项奖励
回复