I have a "mystery" problem.
All my registers for the TC port are set properly:
MCF_GPIO_PTCPAR=0x00;
MCF_GPIO_DDRTC=0x0F;
 
I have no problems to trigger PTC[1], PTC[2] or PTC[3],
but I can not drive PTC[0], pin does not go high when I set
MCF_GPIO_PORTTC=0x01;
or
MCF_GPIO_SETTC=0x01;
I have verified the status of both control registers they are set tot he values I specified for them.
Would could cause this problem?
已解决! 转到解答。
Rich,
Thank you very much for your help.
It appears to be the hardware problem, IC driver on this pin of MP must have been damaged.
When I installed new MCF52233 on the the board this issue have been resolved.
Best regards,
Olga
I have disconnected everything from this pin. Nothing is driven by it.
I tried to put a pull-up resistor (10k to +3.3V) on it, but with the pull-up resistor I can not pull this pin low.
It behaves like it is an input. Though I have configured MCF_GPIO_PTCPAR and MCF_GPIO_DDRTC.
My code is based on ColdFire_Lite7x.
Have you examined the DDR and PAR register, using the debugger, at runtime, to be sure someone has not changed them after you set them, via:
View -> Registers -> General Purpose I/O Port TC Registers
-- Rich
CodeWarrior  does not allow me to view these registers. The only visibility I have is following:
Thread 0X0 (which includes general purpose registers Dn and An) and generic supervisor registers (CACR, ACR0, ACR1, VBR, MBAR, RAMBAR).
I have been using a workaround to verify the status of the registers by introducing an external variable vunit8 temp, and assigning it value of the registers
temp=MCF_GPIO_DDRTC;
and
temp=MCF_GPIO_PTCPAR;
Values that returned are the ones expected.
If you go to your project settings and set:
Debugger -> CF Debugger Settings -> Target Processor
to 52233, then the debugger should be able to display all the processor registers for you.
It makes debugging much easier.
Since that value may be set wrong, it may be good to double check also the processor under:
Language Settings -> ColdFire Assembler -> Processor
Code Generation -> ColdFire Processor -> Target Family
-- Rich
Rich,
Thank you very much for your help.
It appears to be the hardware problem, IC driver on this pin of MP must have been damaged.
When I installed new MCF52233 on the the board this issue have been resolved.
Best regards,
Olga
Is it possible external circuitry is driving the pin?
If you want to verify the HW is connected properly, you could, as a shot in the dark, load StickOS onto the 52233 (from http://www.cpustick.com/downloads.htm) and then use a terminal emulator to connect to (raw) port 1234 of the DHCP IP address assigned to the board... You can then examine and manipulate pins interactively with commands like:
dim x as pin dtin0 for digital output
let x=1
let x=0
There's full documentation for StickOS on that page, as well -- it was designed as an interactive rapid prototyping and education environment. You can see the 52233 Ethernet transport section here: http://www.cpustick.com/stickos.htm#_Toc226454853
-- Rich